DUG_Exxact - Connected Double Socket Outlet 16A_WH-00

Pairing the device with Wiser Hub

Using the Wiser Home app, pair your device with the Wiser Hub to access and control the device.
  1. On the Home screen, tap .
  2. Tap Devices > > Appliances > Connected Socket.
    TIP: You can also navigate by tapping Control > > Appliances > Connected Socket.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.

  4. Tap Next, short press the push button 3 times and make sure that the LED blinks amber.
    Wait for a few seconds until the LED turns green and the app confirms that the device is joined.
  5. Once the device is joined, tap (A) and select an icon suitable for your load and tap Save.
    NOTE: Electric plug icon is assigned by default.
  6. Tap (B) to enter the name of the device.
  7. Tap Next and assign the socket to a new room or an existing room and tap Submit.
    IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.