DUG_LK FUGA Wiser wireless double relay_WH-00

About the device

The LK FUGA® Wiser wireless double relay (hereinafter referred to as relay switch) is a push-button device that can be used to switch LED, ohmic, inductive or capacitive loads manually or remotely.
This device is designed to control two separate loads. The top push buttons operate one load, while the bottom push buttons control the other.

Control options

Home control: To control the relay switch through the Wiser Home app you will need the Wiser Hub.

Direct operation: The relay switch can always be controlled directly on-site. You can also connect any number of mechanical push-buttons to control the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.