DUG_Odace Multiwire Push-button Dimmer_WH-02

Pairing Wireless Switch with Push-button Dimmer

  1. Remove the rocker from the Wireless switch and short press the upper push button (A) 5 times in quick succession.
    The status LED blinks green.
  2. Short press the push-button of the Dimmer 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Push-button Dimmer blinks for a few times. The status LED stops blinking green on the Wireless switch and the Push-button Dimmer. The Push-button Dimmer can now be controlled by the Wireless switch.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.