Pairing the device with the Wiser Hub
- On the Home screen, tap
.
- Tap .
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid.
-
(B): Tap this option if you are unable to find the MAC address and Install code.
-
- Tap Next, remove the rocker of the
Wireless switch and short press the top-right push button (A) 3 times
and make sure that the LED blinks amber.
Wait for a few seconds until the LED turns green and the app confirms that the device is joined.
NOTE: If the LED is blinking green and red, see the instructions by tapping LED blinking green and red? or refer to the Troubleshooting topic. - Tap Next to enter the name of the
device and assign the device to a new room or an existing room.The Wireless switch is now listed on the Control tab under the All and Room tabs.
Hint:
-
If the Wireless switch is configured as 2-gang, and you wish to switch it to 1-gang, you must reset the device and pair it again as a 1-gang.
-
If the Wireless switch is configured as 1-gang, and you wish to switch it to 2-gang, you must reset the device and pair it again as a 2-gang.
For more information, refer to Resetting the device.
-
- Assemble the rocker on the Wireless switch.