DUG_Ovalis Shutter_WH-07

Shutter calibration with Wiser app

The shutter motor is supplied in an uncalibrated state. Each shutter motor varies in the time it takes to complete the opening/closing movement (i.e., edge to edge).

IMPORTANT:
  • It is necessary to select the device type and set the open/close duration before proceeding with shutter calibration. Refer to Selecting device type and Setting configure duration .

  • Do not use the shutter either manually or on the app during calibration to avoid interruption.

  • Follow the procedure for shutter calibration according to the device type: Shutter or Shutter with tilting slats.

Shutter

  1. After setting the open/close duration, go to the Control tab, and tap All devices or the room tab where the device is located.

  2. On the device control screen, drag the sliding bar up/down to set the desired shutter opening percentage (A).

    The shutter opens completely and then it reaches to the desired position set in step 2. The shutter is now calibrated.

Shutter with tilting slats

  1. On the Control tab, tap All devices or the room tab where the device is located.

  2. On the device control screen, in the Position tab, drag the sliding bar up/down to set the desired shutter opening percentage (A).

  3. Tap Slat Tilt, drag the sliding bar up/down to set the desired shutter opening percentage (B) according to any one of the following tilt position:

    • Horizontal

    • Tilted

    • Vertical

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?