DUG_Ovalis Shutter_WH-07

LED Indication

Pairing

User Action

LED Indication

Status

Press the push button 3 times

LED blinks amber per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off.

Resetting

User Action

LED Indication

Status

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED blinks red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks green for a few seconds and then stays amber.

Identifying the device

LED Indication

Status

The LED blinks red.

The shutter opens/closes gradually, upon successful identification of the Blind control switch.

Different connectivity mode

LED Indication

Status

The LED blinks green and red while paring.

The device is trying to connect to other connectivity mode.
Short press the push button 3 times and then hold for 20 seconds. When the LED blinks red rapidly, release the push button.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?