DUG_Ovalis PB Dimmer_WH-07

Switching/Dimming the device manually

You can turn on/off and increase/decrease the brightness of the dimmer manually. The dimmer will provide power to the load connected to it.

Short press the push button (< 0,5 s) once to switch on/off the dimmer.

Long press the push button (> 0,5 s) on the device to increase/decrease the brightness of the dimmer.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?