Configuring the device
|
A |
Device Name: Tap to change the name of the device. |
|
B |
Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. |
|
C |
RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle switch to enable the RL-LED Mode. NOTE: Refer toTechnical Datafor more information.
|
|
D |
LED Indicator Behaviour: Tap to set the LED indicator behaviour of the dimmer as per your preference. Refer to Setting up the LED Indicator Behaviour for detailed information on each options. |
|
E |
Power On Behaviour: Tap to set the default brightness level of the dimmer when it is turned on. Refer to Setting up the Power On Behaviour for detailed information on each options. |
|
F |
Minimum Brightness and Maximum Brightness: This setting lets
you set limits on the maximum and minimum brightness of the connected
load. This is done to avoid flickering and switching off the LED. IMPORTANT: If the light does not
begin to brighten up from 0%, adjust the minimum level setpoint to
the point where the light actually starts to brighten. Similarly,
for maximum brightness, set the maximum level based on the behaviour
of the connected light. For example, if brightness does not increase
between 80% and 100%, then set the maximum level to 80%.
NOTE: The minimum brightness must be lower than the maximum brightness.
|
|
G |
Identify: Tap
to identify the device. The status LED blinks red and connected lighting
devices blinks On/Off, upon successful identification of the dimmer. |
|
H |
Delete: Tap to remove the device from the system. NOTE:
|
|
J |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device. |