DUG_PowerTag-E_WH-10

Disabling Personalised Energy Insights

To disable/stop Personalized Energy Insights services:
  1. On the Home screen, tap   > Account > Apps and Connections > Personalised Energy Insights.
  2. Read the information and tap (A), then tap Stop Service.
    NOTE: To reactivate the service again, follow step 1 menu navigation and tap Personalised Energy Insights. Refer to Enabling Personalised Energy Insights to follow the same procedure.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?