Showing 1 - 7 of 7 results

  • Setting Tariff

    Wiser Home – System User Guide (France)

    Setting Tariff Setting Tariff Setting Tariff You can set tariff in the Wiser Home app to access your energy cost and billing data. The Tariff option available only if you have installed the following energy monitoring device installed at your home. EVlink Home Smart Mureva EVlink Schneider Charge
  • Anti-Tripping Management

    Wiser Home – System User Guide (France)

    a defined limit. The limit value is set by your Contract limit, refer to Setting Tariff. Devices that are eligible will be added automatically to the Anti-Tripping Management. When a device is managed by the Anti-Tripping management, the Schedules, Moments and Automations for that device are not
  • Live

    Wiser Home – System User Guide (France)

    throughout the day. You can interact with the graph to see when the most expensive times are based on your tariff. This graph is displayed only if you set your tariff to Peak/Off-Peak. Refer to Setting Tariff. Import Displays how much power you are importing, a breakdown into consumption categories and a
  • App Settings

    Wiser Home – System User Guide (France)

    billing data. You can set the tariff based on your contract type. Refer to Setting Tariff for detailed information on how to set the tariff. Anti-Tripping Management: To enable/disable the Anti-Tripping Management for devices. The Anti-Tripping Management prevents the circuit breaker from tripping by
  • Wiser Home AI

    Wiser Home – System User Guide (France)

    system . Solar panel monitoring is mandatory if your tariff is set to Flat or Peak/Off-Peak. Without it, the Wiser Home AI feature will not be available. Commission the supported devices. Refer to Pairing the device Power Micromodule EVlink Home Smart EV Socket Schneider Charge Set your tariff according to your electricity contract. Refer to Setting Tariff.
  • Creating an Automation

    Wiser Home – System User Guide (France)

    automation based on changes in energy prices. This trigger is available only if your tariff is set to Peak/Off-Peak. Refer to Setting Tariff. The system manages electricity pricing at a precision of 0.01 €/kWh. Example: The daily average electricity price is 0.24 €/kW. You have set your automation to
  • Wiser Home

    92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Setting Tariff Setting Tariff You can set tariff in the Wiser Home app to access your energy cost and billing data. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Configuring