System User Guide Wiser Home (France) - 14

Live

Provides live data of the grid consumption and live status of where the power is coming from:

  • Grid to Home: Import (Home consuming power from Grid)

  • Home to Grid: Export (Excess power of Solar production fed to Grid)

On the page, tap Live.

A

Displays live data on the power generated by various sources, such as grid, solar panels etc.

IMPORTANT: The live power flow view is intended for quick, real-time checks and not designed to remain open for extended periods. If it stays open for more than a few consecutive minutes, the system will stop updating live data automatically.

B

Indicates the total energy consumption of the household.

C

Lists major categories of devices and their real-time power usage in kilowatts (kW), helping you track energy consumption of each device.

NOTE: If more than four devices are tracked, the energy consumption of the remaining devices will be shown as other loads, representing the total energy consumption of all these devices.

D

Represents energy production throughout the day. Peaks in the graph indicate higher output during specific hours.

E

Provides an overview of your household’s energy performance for the current day, including both energy usage and solar efficiency.

  • Consumption Total: Represents the total amount of energy consumed by the household.

  • Solar Production*: Indicates the total energy generated by the solar panels.

  • Self-Sufficiency*: Shows the percentage of total energy consumption that was covered by self-generated solar power, reflecting how independent the household is from external energy sources.

  • Production Used*:  Indicates the percentage of solar energy produced that was actually used by the household.

NOTE: * Indicates that these data are available only for On-Grid solar systems.

F

Displays the real-time electricity pricing throughout the day. You can interact with the graph to see when the most expensive times are based on your tariff.

NOTE: This graph is displayed only if you set your tariff to Peak/Off-Peak. Refer to Setting Tariff.

Import

Displays how much power you are importing, a breakdown into consumption categories and a consumption timeline.

Import and Export (Applicable for Grid with On Grid solar system)

Displays how much power you are importing or exporting, a breakdown into consumption categories and a consumption time line.

The grid consumption with loads is represented in blue and the excess power of battery and solar is represented in green.

NOTE: Scroll down in the app to view the complete graph.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.