System User Guide Wiser Home (France) - 14

App Settings

Overview of the options available in the settings menu.

The settings menu contains various settings for parts of the Wiser Home System.

Rooms and Devices are managed from the settings menu.

On the Home Screen:

  1. Tap .

    The settings menu:

    Account

    Change the details of your account, like password, notification settings, home address, etc.

    NOTE: You can also find the notification settings (e.g. Battery low) here.

    Energy Management

    This option is available only if you have Energy devices installed at your home.

    • Tariff: Set the tariff to access your energy cost and billing data. You can set the tariff based on your contract type. Refer to Setting Tariff for detailed information on how to set the tariff.

    • Anti-Tripping Management: To enable/disable the Anti-Tripping Management for devices. The Anti-Tripping Management prevents the circuit breaker from tripping by switching off the load (e.g. Water Heater, EV Socket) or reducing the power of the load. Devices that are eligible will be added automatically to the Anti-Tripping Management. Refer to Anti-Tripping Management for detailed information on how to enroll the Anti-Tripping management.

    • Wiser Home AI: You can enroll/disenrol the devices or edit the home profile whenever required. The Wiser Home AI feature allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EVlink socket ) or resistive Water boilers (controlled with a Power Micromodule). Refer to Wiser Home AI for detailed information on Reduce my Bill.

    Rooms

    List of all Rooms of your Home. Access to Room options.

    Devices

    List of all Devices of your Home. Access to Device options.

    Away Mode

    Specify what happens when you activate the Away Mode, like temperature setting and which devices should be switched off. Refer to Away Mode for detailed information.

    Smart Modes

    Activate or deactivate the Smart Modes, like ECO Mode.

    System Settings

    More detailed Wiser Home App information. Set your time zone here.

    Support

    Provides you the general assistance such as the link to the FAQ section of se.com, access detailed guide, report errors, and provides contact information for customer support. Refer to Support for the detailed information.

    Home Screen

    Customize the appearance of the Home Screen.

    App Theme

    Personalize the appearance of Wiser home app to light mode or dark mode. Refer to App Theme.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.