Showing 1,041 - 1,050 of 1,622 results

Page 105 of 163
  • Changing the orientation of outside temperature sensors

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    temperature sensors: In the Seasonal Comfort Mode set-up page, tap Outside temp sensors. Tap to see the available outside temperature sensors in Wiser Home app. Select the orientation in which the outside temperature sensors are facing and tap Set.
  • Changing the orientation of outside temperature sensors

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    temperature sensors: In the Seasonal Comfort Mode set-up page, tap Outside temp sensors. Tap to see the available outside temperature sensors in Wiser Home app. Select the orientation in which the outside temperature sensors are facing and tap Set.
  • Changing the orientation of outside temperature sensors

    Exxact - Connected Blind Control Switch – Wiser Home Device user guide

    temperature sensors: In the Seasonal Comfort Mode set-up page, tap Outside temp sensors. Tap to see the available outside temperature sensors in Wiser Home app. Select the orientation in which the outside temperature sensors are facing and tap Set.
  • Wiser Smoke Alarm - 230 V Wiser Home Device user guide

    supplied. Other smoke alarms are considered as Secondary. 2. Short press the Test/Hush button 3 times within 2 s on the primary smokealarm. The Standby LED turns on for 30 s once it is in pairing mode.3. Identify a Secondary smoke alarm and short press the Test/Hush button 3 times within 2 s.The Standby
  • Schedules

    Wiser Home – System User Guide (France)

    schedule. For a detailed understanding of which action/control mode takes precedence over others, refer to Understanding Control Mode Priorities . Schedules are created and edited on the Automation screen (A) Tap a Schedule to navigate to the Schedule details. Schedule details: A Device type A Schedule can
  • Création d’un programme/évènement

    Odace - Thermostat connecté filaire 2 A – Guide de l'utilisateur de l’appareil Wiser Home

    pour ajouter un évènement: Sélectionnez la température (par exemple 16°C). Quand vous placez le curseur au bas de la barre pour le programme, le mode Protection contre le gel est activé lorsque le programme commence.En mode Protection contre le gel, le système maintient la température dans la pièce à 5
  • Creating a Schedule/Event

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    schedule, Frost Protection Mode will activate when the schedule begins. In Frost Protection Mode, the system maintains the room temperature at 5 °C to prevent freezing. WHEN: Set the time for the event (for example 12:00) You can create a maximum of 8 events per day. Copy Schedule: You can tap to copy
  • Changer l’orientation des capteurs de température extérieure

    Unica - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    l’orientation des capteurs de température extérieure : Dans la page de configuration du Mode Confort Saisonnier, appuyez sur Capteurs de température extérieure. Appuyez sur pour voir les capteurs de température extérieure disponibles dans l’application Wiser Home. Sélectionnez l’orientation dans laquelle les capteurs de température extérieure sont installés et appuyez sur Enregistrer.
  • Creating an automation

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Création d’un automatisme

    Wiser micromodule pour interrupteur – Guide de l'utilisateur du dispositif Wiser Home

    Ajouter des conditions (B) et sélectionnez l’une des options suivantes (C) : Changement d’état d’un équipement (sélectionnez l’appareil) : Un automatisme est déclenché en fonction de l’état d’un appareil, tel que l’ouverture d’un volet ou la détection d’un mouvement par un capteur de mouvement. Mode
Page 105 of 163