DUG_Exxact - ZB Thermostat 16 A_WH-01

Creating a Schedule/Event

Schedule/Event allows you to control how your thermostat behaves throughout the day. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.

  1. On the Home screen, tap .

  2. Tap Schedules tab > .

  3. On the New Schedule page, enter the Schedule name, select TYPE, and select room.

  4. Tap Create.

  5. Select any day (A) and tap to add an event:

    • TEMPERATURES: Select the desired temperature (for example 16 °C).

      NOTE: If you move the slider to the bottom of the bar for the schedule, Frost Protection Mode will activate when the schedule begins. In Frost Protection Mode, the system maintains the room temperature at 5 °C to prevent freezing.
    • WHEN: Set the time for the event (for example 12:00)

      NOTE: You can create a maximum of 8 events per day.

      Copy Schedule: You can tap to copy the schedule from one day to other days or copy the entire schedule to a new schedule or to an existing one.

  6. Tap Set.

  7. On the top-right corner of the screen, tap and select Follow schedule toggle switch to turn on/off the schedule.

How setpoint changes work

When your system is following a schedule:

  • The new setpoint remains active until the next scheduled event.

  • You can view the time until which a schedule is active, on the Control tab under the device name. This indicates how long the current schedule will stay ON.



When your system is not following a schedule:
  • Any changes made using the slider remains active until you adjust the slider again.

  • The time until which a schedule is active will not be displayed on the screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?