Showing 1,061 - 1,070 of 1,622 results

Page 107 of 163
  • Changing the orientation of outside temperature sensors

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    temperature sensors: In the Seasonal Comfort Mode set-up page, tap Outside temp sensors. Tap to see the available outside temperature sensors in Wiser Home app. Select the orientation in which the outside temperature sensors are facing and tap Set.
  • Changing the orientation of outside temperature sensors

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    temperature sensors: In the Seasonal Comfort Mode set-up page, tap Outside temp sensors. Tap to see the available outside temperature sensors in Wiser Home app. Select the orientation in which the outside temperature sensors are facing and tap Set.
  • Affichages LED

    Wiser Actionneur de Chauffage électrique pour la commande de température – Guide de l’utilisateur de l’appareil

    et vert en alternance Non appairé LED éteinte : chauffage à l’arrêt LED orange fixe : chauffage activé Mode dégradé(pas de connexion avec le thermostat ou avec la passerelle) Clignotement rouge : chauffage à l’arrêt LED rouge fixe : chauffage activé Test/forçage manuel Clignotement vert : chauffage activé en raison du forçage
  • Creating an automation

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Creating an automation

    Odace - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Création d’un automatisme

    Odace - Variateur rotatif connecté universel LED 2fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    . Mode Absence (activez ou désactivez) : Le mode Absence peut également déclencher un automatisme pour allumer les lumières, fermer les volets, etc. Reportez-vous à la rubrique Mode Absence dans le Guide de l’utilisateur du système correspondant. Vous pouvez ajouter jusqu’à 10 conditions. Dans cet
  • Creating an automation

    LK One Wiser Multiwire LED Rotary Dimmer – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    EVlink Home Smart – Wiser Home device user guide

    Add conditions (C) and select any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Energy Price changes (To define the energy price limit.) This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum
  • Création d’un automatisme

    Ovalis - Interrupteur variateur universel LED connecté – Guide de l'utilisateur de l'appareil domestique Wiser

    . Mode Absence (activez ou désactivez) : Le mode Absence peut également déclencher un automatisme pour allumer les lumières, fermer les volets, etc. Reportez-vous à la rubrique Mode Absence dans le Guide de l’utilisateur du système correspondant. Vous pouvez ajouter jusqu’à 10 conditions. Dans cet
  • Création d’un automatisme

    Unica - Interrupteur à relais 10 A connecté – Guide de l'utilisateur du dispositif Wiser Home

    Ajouter des conditions (B) et sélectionnez l’une des options suivantes (C) : Changement d’état d’un équipement (sélectionnez l’appareil) : Un automatisme est déclenché en fonction de l’état d’un appareil, tel que l’ouverture d’un volet ou la détection d’un mouvement par un capteur de mouvement. Mode
Page 107 of 163