Showing 121 - 130 of 1,457 results

Page 13 of 146
  • Creating an automation

    LK FUGA Wiser Push-button Switch – Wiser Home Device user guide

    be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User
  • Creating an automation

    LK FUGA® Wiser wireless double relay – Wiser Home Device User Guide

    be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User
  • Creating an automation

    EVlink Home Smart – Wiser Home device user guide

    Add conditions (C) and select any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Energy Price changes (To define the energy price limit.) This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. Maximum
  • Creating an automation

    Ovalis - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    Unica - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    Odace - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • Creating an automation

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. For more
  • Creating an automation

    Odace - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor. Away Mode (Enable or Disable): Away mode can also trigger an automation to turn on the lights, close the shutter etc. Refer to the Away Mode topic in the respective System
  • LED Indications

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees. Away mode Status User Interaction Description Away mode is set in Wiser Home app. A dot-matrix display glows, indicates that the thermostat is in away mode.
  • Creating an automation

    Exxact - Connected Motion Sensor with Push-button Dimmer LED – Wiser Home Device user guide

    . Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User Guide. Tap Device status change > Motion Dimmer and select any of the following options: Dimmer On / Off: Select the dimmer
Page 13 of 146