DUG_Exxact - ZB Thermostat 16 A_WH-01

LED Indications

Pairing the device

Status

User Interaction

Description

Pairing in progress

The thermostat matrix display flashes "Jn" to indicate joining is initiated when the thermostat O touch button is pressed and held for > 3 s.

Successful joining network

The thermostat matrix display flashes a green LED when the thermostat successfully joins a network.

Fails to join the network

The thermostat matrix display flashes a red LED when the thermostat fails to join the network.

Presetting the device

Status

User Interaction

Description

Enter preset selection

By default, thermostat matrix display flashes “P5” if there is no external sensor connected, or “P8” if there is any external sensor connected when the thermostat is first powered on or after a factory reset.

Modify preset selection

The default preset value can be modified by simultaneously pressing "O" and "+" for 2 s to enter advanced settings menu In advance setting menu the thermostat matrix display flashes "P1" or "P2...P9" when +/– button is pressed.

Note: When + button is pressed, preset increases by one; similarly, the preset decreases by one when the button is pressed.

For more information, refer to the section presetting the device.

Setting a sensor type

Status

User Interaction

Description

Floor sensor type selection

The thermostat matrix display the floor sensor type and LED flashes blue.

Floor sensor calibration.

The thermostat matrix display calibration value and LED flashes purple.

Floor temperature maximum limit

The thermostat matrix display maximum temperature limit and LED flashes red.

Resetting the device

Status

User Interaction

Description

Soft reset

A solid "Sr" LED is displayed on the thermostat matrix display until the user releases the O button, then "Sr" flashes. For more information, refer to the section Resetting the device.

Factory reset

A solid "Fr" LED is displayed on the thermostat matrix display until the user releases the O button, then "Fr" flashes. For more information, refer to the section Resetting the device.

Showing demand - temperature control modes

Status

User Interaction

Description

Heating demand

The LED flashes white at 1hz during heating demand.

Temperature display

Status

User Interaction

Description

Temperature below minimum display value
OR
Temperature reading error.

Note: The thermostat matrix displays temperature limits -9 °C to 99 °C.

The thermostat matrix display flashes “--” When the temperature is below -9 degrees.

OR

The thermostat matrix display flashes “--” when the thermostat cannot determine the temperature due to an error.

Temperature above maximum display value

Note: The thermostat matrix displays temperature limits -9 °C to 99 °C.

The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees.

Away mode

Status

User Interaction

Description

Away mode is set in Wiser Home app.

A dot-matrix display glows, indicates that the thermostat is in away mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?