Showing 1,271 - 1,280 of 1,648 results

Page 128 of 165
  • Ovalis - Connected Relay Switch 10 A

    Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Setting the device location Setting the device location You can add your device to any room (such as bedroom, living room, dining room etc.). Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France
  • Relay Cycle Time

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Relay Cycle Time Relay Cycle Time Relay Cycle Time In advanced settings, you can choose Relay Cycle Time (A). This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle
  • Configuring the bottom push buttons

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    configure a specific device state, such as turning lights on or off, moving shutters up or down, or setting a specific brightness or shutter position (for example, 50% brightness or 30% open). Moment: Moment allows you to group multiple actions that are usually performed together. By using the Wiser Home app, you can create moments based on your needs.
  • System M und System D - Connected SCHUKO-Steckdose 16 A Wiser Home Geräte-Benutzerhandbuch

    während derInstallation des PowerTags eingestellte Netz-Wert nicht mit dem Tarifübereinstimmt. Weitere Informationen finden Sie unter Setting Tariff. • Koppeln Sie die unterstützten Geräte. Siehe Gerät koppeln (je nachdem,welche Geräte Sie installiert haben) - Lastaktor, EV-Steckdose, Smart Plug
  • Using the device

    Ovalis - Connected Relay Switch 10 A – Wiser Home Device user guide

    Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
  • Using the device

    Exxact - Connected Relay Switch 10 A – Wiser Home Device user guide

    Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
  • Amazon Alexa

    Wiser Home – System User Guide (Denmark)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Exxact - Connected Double Socket Outlet 16A Wiser Home Device user guide

    . You can enrollup to eight loads at a time, which helps maintain the total consumption of thesystem below the established limit. This limit is determined by your contractspecifications, so it's important to refer to the Setting Tariff section for informationon peak and off-peak rates. Eligible devices
  • Using the device

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
  • Using the device

    Odace - Connected Relay Switch 10 A – Wiser Home Device user guide

    Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
Page 128 of 165