DUG_LK FUGA Wiser wireless dimmer_WH-00

Configuring the bottom push buttons

You can configure an action or moment for the push buttons. Pressing a push button allows you to operate connected devices based on the assigned function.
  • Action: Action allows you to configure a specific device state, such as turning lights on or off, moving shutters up or down, or setting a specific brightness or shutter position (for example, 50% brightness or 30% open).

  • Moment: Moment allows you to group multiple actions that are usually performed together. By using the Wiser Home app, you can create moments based on your needs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.