Showing 1,291 - 1,300 of 1,648 results

Page 130 of 165
  • Using the device

    Exxact - Connected Relay Switch 10 A – Wiser Home Device user guide

    Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. C Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. D Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device.
  • Amazon Alexa

    Wiser Home – System User Guide (France)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Amazon Alexa

    Wiser Home – System User Guide (Germany, Austria)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Amazon Alexa

    Wiser Home – System User Guide (UK, Ireland)

    setpoint change if that change is to occur in under an hour. After that it goes back to its original setting, and you must tell Alexa to do it again. If a Device is following a Schedule, any setting changed by Alexa will last until the next event in the Schedule. If the Device is running in manual mode
  • Technical Data

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Power supply 2 x 1.5 V IEC LR6 (AA) alkaline batteries or 2 x HR6 NiMH batteries Without power supply: Connection data are retained Temperature setting range 5 °C - 30 °C Temperature resolution 0.5 °C Control accuracy < 0.8 °C at 4 °C/h Surface
  • About the device

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    maximum of 10 mechanical double push-button switches. Protection of the motor against damage, using two mutually mechanical and electronic locks between the relay contacts. Protection against electronic overload, overheating and short-circuit. Setting a schedule using Wiser app.
  • LED indications

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    . Setting (Default state) LED Indication Description The Red LED glows. The Red LED glows when the output is switched ON. All the LEDs are OFF. The LEDs are OFF, when the output is OFF. Alarms LED Indication Description Blinking red fast When there is an overload or over-temperature alarm and the device is switched off. Refer to the Troubleshooting to clear the alarms.
  • Creating a moment

    LK FUGA Wiser Push-button Switch – Wiser Home Device user guide

    actions menu, you can select the devices (C). Once devices are selected, tap Done. On the Moment creator page, tap the device to set the condition. For example, if it is a relay switch: Tap to turn on (D) and tap Set on the top-right screen. After setting all conditions, tap Save. Once the moment is
  • Creating a moment

    Exxact - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    actions menu, you can select the devices (C). Once devices are selected, tap Done. On the Moment creator page, tap the device to set the condition. For example, if it is a Motion Sensor Switch: Tap to turn on (D) and tap Set on the top-right screen. After setting all conditions, tap Save. Once the
  • Assigning actions to push buttons

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    Assigning actions to push buttons Assigning actions to push buttons Assigning actions to push buttons You can configure an action to the push buttons, such as turning lights on or off, moving the shutter up or down, or setting a combination of functions. On the Control tab, tap All devices or the
Page 130 of 165