DUG_LK FUGA Wiser wireless dimmer_WH-00

Assigning actions to push buttons

You can configure an action to the push buttons, such as turning lights on or off, moving the shutter up or down, or setting a combination of functions.
  1. On the Control tab, tap All devices or the room tab where the dimmer is located.
  2. Tap > Configure buttons.
  3. Tap any key and select Action.
  4. Select the device as per your preference and tap Select Action. For example, select Light Switch.
  5. On the Configure Device screen, tap Light Switch.
  6. Tap to turn on the light and tap Set > Set Action.

    In the next screen, shows that the Action is successfully configured.

    The Push Button 1 key is configured with Light Switch: On

    TIP: When assigning a push button to control a dimmer or shutter, you can set a specific brightness level or shutter position, for example, 50% brightness for the light or 30% opening for the shutter. These actions are triggered by a short press only. Press and hold is not supported for dimming or shutter movement.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.