Showing 1,301 - 1,310 of 9,870 results

Page 131 of 987
  • Operating a Dimmer

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    Operating a Dimmer Operating a Dimmer Operating a Dimmer You can switch the dimmer ON/OFF and adjust its brightness using the paired Wireless switch. Short press the top (ʌ+) or bottom (v-) of the Wireless switch (< 0,5 s) to turn ON/OFF the connected load (A). Long press the top (ʌ+) or bottom (v-) of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).
  • Operating a Dimmer

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Operating a Dimmer Operating a Dimmer Operating a Dimmer You can switch the dimmer ON/OFF and adjust its brightness using the paired Wireless switch. Short press the top (ʌ+) or bottom (v-) of the Wireless switch (< 0,5 s) to turn ON/OFF the connected load (A). Long press the top (ʌ+) or bottom (v-) of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).
  • Deleting a schedule

    Ovalis - Connected Relay Switch 10 A – Wiser Home Device user guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Deleting a Schedule

    Wiser Home – System User Guide (Germany, Austria)

    Deleting a Schedule Deleting a Schedule Deleting a Schedule On the Schedule details screen: Tap Delete (A). The Wiser Home App automatically creates a default Schedule for Climate control devices. If the Wiser Hub has to be reset, the Wiser Home app will again create a default Schedule for all
  • Substituir a bateria

    Sensor temperatura/humidade Wiser – Guia do utilizador do dispositivo Wiser Home

    Substituir a bateria Substituir a bateria Substituir a bateria Remova o sensor da placa base deslizando-o para cima. Desparafuse a tampa da bateria usando uma chave de fenda. Substitua a bateria pela polaridade adequada. Reinstale a tampa da bateria e aperte o parafuso usando uma chave de fenda. O
  • Deleting a schedule

    Odace - Connected Relay Switch 10 A – Wiser Home Device user guide

    Deleting a schedule Deleting a schedule Deleting a schedule On the Home screen, tap Automations Schedules. Tap the schedule you want to delete. Tap SCHEDULE DETAILS, tap Delete, and then select OK.
  • Operating a Dimmer

    Wiser Multiwire Micro Module LED Dimmer – Wiser Home device user guide

    Operating a Dimmer Operating a Dimmer Operating a Dimmer You can switch the dimmer on/off and adjust its brightness using the paired Wireless switch. Short press the top or bottom of the Wireless switch (< 0,5 s) to turn on/off the connected load (A). Long press the top or bottom of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).
  • Editing a schedule

    PowerTag Control – Device user guide

    Editing a schedule Editing a schedule Editing a schedule You can edit an existing schedule according to you preference. On the Home screen, tap Automations . Tap the schedule you want to edit. Tap the SCHEDULE DETAILS and you can do the following actions: Rename the schedule (A). Within the Applies
  • Deleting a Schedule

    Wiser Home – System User Guide (Sweden, Finland)

    Deleting a Schedule Deleting a Schedule Deleting a Schedule On the Schedule details screen: Tap Delete (A). The Wiser Home App automatically creates a default Schedule for Climate control devices. If the Wiser Hub has to be reset, the Wiser Home app will again create a default Schedule for all
  • Editing a Schedule

    Wiser Home – System User Guide (UK, Ireland)

    Editing a Schedule Editing a Schedule Editing a Schedule In the Schedule details screen: Tap (A) icon to change the name of the Schedule. Select the Devices (B) the Schedule applies to. Select the day (C) you want to add or edit events. Tap (D) icon to edit an event. Tap (E) icon to add an event to
Page 131 of 987