Showing 141 - 150 of 1,622 results

Page 15 of 163
  • Activity and environment

    Wiser Home – System User Guide (France)

    you turned your heating down is counted by a manual boost or boost down. Number of times you turned your heating up is counted by a boost up or manual adjustment to the temperature. Number of hours of sunshine is calculated as number of hours when the cloud coverage was less than 50%.
  • Activity and environment

    Wiser Home – System User Guide (Spain and Portugal)

    you turned your heating down is counted by a manual boost or boost down. Number of times you turned your heating up is counted by a boost up or manual adjustment to the temperature. Number of hours of sunshine is calculated as number of hours when the cloud coverage was less than 50%.
  • LED indications

    Wiser Radiator Thermostat – Wiser Home Device user guide

    LED indications LED indications LED indications Normal use State User Interaction Left LED Center LED Right LED Duration Boost up Twist the cap in the + direction Solid for 5 seconds Boost down Twist the cap in the - direction Solid for 5 seconds Head calibration State User Interaction Left LED
  • Aktivität und Umgebung

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    Heizung heruntergedreht haben, wird durch manuellen Boost oder Boost-Down gezählt. Wie oft Sie Ihre Heizung hochgedreht haben, wird durch einen Boost-Up oder eine manuelle Temperatureinstellung gezählt. Die Anzahl der Sonnenstunden wird als die Anzahl der Stunden berechnet, in denen der Bewölkungsgrad unter 50 % lag.
  • Creating an automation

    Wiser Room Thermostat – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Creating an automation

    Wiser-lämpötila-/kosteusmittari – Wiser Home -laitteen käyttöopas

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Creating an automation

    Wiser Temperature/Humidity Sensor – Wiser Home Device user guide

    Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away
  • Wiser Flush-mounted Thermostat 2 A

    in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Boost All Boost All You can apply a boost of +2 °C for 1 hour to every room in the system. It won’t affect hot water in any way
  • Activity and environment

    Wiser Home – System User Guide (Germany, Austria)

    you turned your heating down is counted by a manual boost or boost down. Number of times you turned your heating up is counted by a boost up or manual adjustment to the temperature. Number of hours of sunshine is calculated as number of hours when the cloud coverage was less than 50%.
  • Updating the Installer Portal

    Schneider Inverter and Boost – Wiser Home Device user guide

    the left menu, click ⊕ Add Site. Enter the required information and then click Add Site. Change the language from the menu in the top right. Configuring export mode By default, zero export mode is enabled. In zero export mode, the Schneider Inverter does not export any power to the grid. The maximum
Page 15 of 163