Showing 191 - 200 of 328 results

Page 20 of 33
  • Exxact - Connected Thermostat Room/Floor 16 A

    Deleting an automation Deleting an automation Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric
  • Troubleshooting in Quick Home Connect

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    module light switch Micro module shades control Multiwire micro module dimmer Push–button dimmer Socket outlet Relay switch Blind control switches Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in
  • Troubleshooting in Quick Home Connect

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    module light switch Micro module shades control Multiwire micro module dimmer Rotary dimmer Push-button dimmer Socket outlet Relay switch Blind control switches Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the
  • Creating an automation

    Wiser Power Micromodule – Device user guide

    condition must be met to trigger an automation. Tap Add conditions (C) and select any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Maximum 10 conditions can be added. Select a device (E) that will set the condition and then select Instant power (F). Tap
  • Renova - Connected Thermostat Room/Floor 16 A

    Deleting an automation Deleting an automation Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric
  • Creating an automation

    PowerTag Energy – Wiser Home device user guide

    any of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Maximum 10 conditions can be added. Select a device that will set the condition. In this example, select Grid. Tap more than (E) and enter a power value in field (F). Tap Set (G). To remove an added
  • Creating an automation

    Mureva EVlink – Device user guide

    change (Select the device) Away Mode (Enable or Disable) Maximum 10 conditions can be added. Select a device (E) that will set the condition. Tap the device icon state (On/Off) to set an action and tap Set. To remove an added condition, swipe left and tap . Then add a new condition with the required
  • Creating an automation

    Wiser Micromodule for Fil Pilote radiators – Device user guide

    following (D): Device status change (Select the device) Away Mode (Enable or Disable) Maximum 10 conditions can be added. Select a device (E) that will set the condition and then select Set point (F). Select less than (G) and drag the sliding bar (H) up/down to set the temperature. To remove an added
  • Wiser Home System User Guide (Germany, Austria)

    signalstrength. Tap a Device in the List to navigate to the Device Details, page 69. 1. Login to the app. 2. On the Home Screen, tap . Control InsightHome Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay
  • Wiser Flush-mounted Thermostat 2 A

    ) 1 41 29 70 00 Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric 35 rue Joseph Monier 92500 Rueil
Page 20 of 33