Showing 21 - 30 of 1,622 results

Page 3 of 163
  • Away Mode

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    . When Away mode is active, only rooms that have set point temperatures higher than the Away mode temperature will be affected. For example, if a given room is set to 5 °C, Away mode will not force it to the Away temperature. While Away Mode overrides Boost and rooms that are and aren’t following a
  • Built in Automation

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Built in Automation Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode.
  • Built-in Automation

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Built-in Automation Built-in Automation Built-in Automation There are three built-in Automation such as Boost All, Cancel all overrides and Away mode.
  • Automatismes intégrés

    Odace - Thermostat connecté filaire 2 A – Guide de l'utilisateur de l’appareil Wiser Home

    Automatismes intégrés Automatismes intégrés Automatismes intégrés Trois automates sont intégrés, tels que Boost All, Cancel all overrides et Away mode.
  • Built in Automation

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    Built in Automation Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode.
  • Built-in Automation

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Built-in Automation Built-in Automation Built-in Automation There are three built-in Automation such as Boost All, Cancel all overrides and Away mode.
  • Setting the room temperature using the app

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Setting the room temperature using the app Setting the room temperature using the app Setting the room temperature using the app Using the Wiser Home app, you can adjust, set or boost the room temperature. Precondition: Add a Wiser Room Thermostat/ Wiser Temperature/Humidity Sensor in the same room
  • Built in Automation

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    Built in Automation Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode.
  • Operating modes

    Wiser Micromodule for Fil Pilote radiators – Wiser Home Device User Guide

    indicates the mode in which the system is working. Off : Turns the system off, available in Home screen. Heating : System operates in heating mode when the set-point temp > room temp. Boost mode : Boost Mode will apply a boost of +2 °C for one hour to every room in the system. For more
  • Away Mode

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    . When Away mode is active, only rooms that have set point temperatures higher than the Away mode temperature will be affected. For example, if a given room is set to 5 °C, Away mode will not force it to the Away temperature. While Away Mode overrides Boost and rooms that are and aren’t following a
Page 3 of 163