DUG_Wiser_Micromodule for Fil Pilote radiators_WH-05

Operating modes

Using the Wiser Home app, you can control the Heating devices.
  1. On the Control tab, tap All devices or a room tab where the Plug is located > Heating device.
  2. On the Device Control screen, the current temperature is shown.
    The current operating mode indicates the mode in which the system is working.
    • Off : Turns the system off, available in Home screen.
    • Heating : System operates in heating mode when the set-point temp > room temp.
    • Boost mode: Boost Mode will apply a boost of +2 °C for one hour to every room in the system. For more information on different modes, refer to Wiser Modes.
    NOTE: To access live, history and energy insights, it’s recommended to install PowerTag on the module loads. Refer to Checking device consumption.

    TIP: You can also turn the device ON/OFF when you add it to your Favourites. To know more about Favourites, refer to the Manage Favourites topic in the respective System User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?