Setting the room temperature using the app
Precondition: Add a Wiser Room Thermostat/Wiser Temperature/Humidity Sensor in the same room where Thermostat is located.
To adjust, set or boost the room temperature:
-
On the Control tab, tap All devices or a room tab where the Thermostat is located.
-
Use the slider control on the right of the screen to adjust the temperature.
NOTE: The flame shows that the room temperature is lower than the desired temperature (set point) and so the heating is ON.IMPORTANT:-
When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point.
-
Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.
TIP: You can also adjust the room temperature:NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen. -
-
IMPORTANT: Once the boost time is set, the set-point temperature automatically increases by 2 °C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.
-