Showing 201 - 210 of 1,429 results

Page 21 of 143
  • Wiser Home System User Guide (Germany, Austria)

    signalstrength. Tap a Device in the List to navigate to the Device Details, page 75. 1. Login to the app. 2. On the Home Screen, tap . Control InsightHome Good evening Favourite devices Edit Motion SensorHallway Critical battery Unoccupied Moments Edit Away Mode Good night Tips and advice See all Stay safe and
  • LK FUGA® Wiser wireless PIR dimmer with neutral Wiser Home Device user guide

    turn on/off the device on the Device Control Screen, tap (B) to turn on/off the Motion Sensor Dimmer. Away ModeAway Mode automatically turns off the Motion Sensor Dimmer. For example, whenyou are away from home for a long time, the light should not turn on due to falsemotion detections. This
  • System M and System D - Connected Thermostat 16 A, ZB

    00 www.se.com Schneider Electric Built in Automation Built in Automation There are three built in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Boost All Boost
  • Renova - Connected Thermostat Room/Floor 16 A Wiser Home Device User Guide

    : Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information about AwayMode , refer to the System User Guide. 5. Tap Device status change
  • Wiser Home AI

    Wiser Home – System User Guide (Germany, Austria)

    to activate or deactivate loads. Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions
  • Wiser Home AI

    Wiser Home – System User Guide (Denmark)

    to activate or deactivate loads. Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions
  • Wiser Flush-mounted Thermostat 2 A

    in Automation such as Boost All, Cancel all overrides and Away mode. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Boost All Boost All You can apply a boost of +2 °C for 1 hour to every room in the system. It won’t affect hot water in any way
  • Modo Ausente

    Unica - Detector de movimiento con interruptor 10A conectado – Guía del usuario del dispositivo Wiser Home

  • Wiser Home AI

    Wiser Home – System User Guide (Sweden, Finland)

    to activate or deactivate loads. Temporary Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions
  • Exxact - Connected Thermostat Room/Floor 16 A Wiser Home Device User Guide

    by adding a condition that will triggeryour automation. B A DUG_Exxact - ZB Thermostat 16 A_WH-01 41 Exxact - Connected Thermostat Room/Floor 16 A 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away
Page 21 of 143