Showing 211 - 220 of 1,622 results

Page 22 of 163
  • Away Mode

    Exxact - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    Away Mode Away Mode Away Mode Away Mode automatically turns off the Motion Sensor Switch. For example, when you are away from home for a long time, the light should not turn on due to false motion detections. This feature ensures the device remains off even if motion is detected, helping to save
  • Affichages LED

    Wiser Tête de Vanne Thermostatique – Guide de l'utilisateur de l’appareil Wiser Home

    signal Tournez le capuchon dans le sens + pour démarrer un boost. Clignotement rapide pendant 5 secondes (répété) Pas de signal Tournez le capuchon dans le sens - pour démarrer un boost. Clignotement rapide pendant 5 secondes (répété) Aucun réseau Tournez le capuchon dans le sens + ou - pour démarrer
  • Commande du chauffage

    Wiser Home – Guide de l’utilisateur du système (France)

    thermostatique ne doit pas effectuer de boost et doit afficher le même état qu’en mode de verrouillage de l’appareil. Le thermostat d’ambiance doit se réveiller à l’aide de l’une des 3 touches (+, -, O), mais les pressions ultérieures de bouton ne modifieront pas la valeur de consigne. L’eau chaude
  • Eco Mode

    Wiser Home – System User Guide (Germany, Austria)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
  • Charging mode

    Mureva EVlink – Wiser Home Device User Guide

    Charging mode Charging mode Charging mode Using the Wiser Home app, you can manage the mode of charging. On the Control tab, tap All devices > Mureva EVlink Socket. On the device control panel page, tap Charging Mode. On the EV Charging Mode menu, select one of the following: Manual: To initiate
  • Comfort Mode

    Wiser Home – System User Guide (Spain and Portugal)

    Comfort Mode Comfort Mode Comfort Mode Comfort Mode is a smart feature that helps ensure the set-point temperature is reached by the time the heating is scheduled to turn ON. It enhances thermal comfort by adjusting the setpoint ahead of schedule, ensuring the room reaches the desired temperature
  • Charging mode

    Schneider Charge – Wiser Home Device user guide

    Charging mode Charging mode Charging mode Using the Wiser Home app, to manage the mode of charging. On the Control tab, tap All devices > Schneider Charge. On the device control panel page, tap Charging Mode. On the EV Charging Mode menu, select one of the following: Manual: To initiate the
  • Away Mode

    Wiser Home – System User Guide (Belgium)

    Away Mode Away Mode Away Mode The Away Mode is designed to set your home in a sensible state when you are away for longer periods (e.g. being away for the weekend). It temporarily overrides the normal controls (e.g. moments, automation) implemented in the hub. When you disable away mode, the
  • Comfort Mode

    Wiser Home – System User Guide (UK, Ireland)

    Comfort Mode Comfort Mode Comfort Mode Comfort Mode is a smart feature that helps ensure the set-point temperature is reached by the time the heating is scheduled to turn ON. It enhances thermal comfort by adjusting the setpoint ahead of schedule, ensuring the room reaches the desired temperature
  • Away Mode

    Unica - Connected Motion Sensor with Dimmer LED – Wiser Home Device user guide

    Away Mode Away Mode Away Mode Away Mode automatically turns off the Motion Sensor Dimmer. For example, when you are away from home for a long time, the light should not turn on due to false motion detections. This feature ensures the device remains off even if motion is detected, helping to save
Page 22 of 163