Showing 231 - 240 of 328 results

Page 24 of 33
  • Exxact - Connected Multiwire Universal Rotary Dimmer LED Wiser Home Device user guide

    and the device again. Refer to• Rotary dimmer, page 8 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer
  • Exxact - Connected Multiwire Universal Push-button Dimmer LED Wiser Home Device user guide

    control thedevice reliably. The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Push–button dimmer, page 8 The Wireless switch battery is discharged. Replace the
  • LK FUGA® Wiser Multiwire LED Rotary Dimmer Wiser Home Device User Guide

    Wireless switch and the deviceare too far away from each other. Place the Wiser Wireless switch in a positioncloser to the device. The Wiser Wireless switch lost pairing. Pair the device again. Refer to• Rotary dimmer, page 9 The Wiser Wireless switch battery isdischarged. Replace the battery of the
  • Odace - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Socket outlet, page 9 The Wireless switch battery is discharged. Replace the battery of the Wireless switch Scenario Procedure Control multiple
  • Unica - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    Symptom Possible cause Solution LED displays amber on the device. Pairing not completed and returned to factorydefault. Pair the Wireless switch and the device again. Refer to• Socket outlet, page 9 Wireless switch not able to control thedevice reliably. The Wireless switch and the device are toofar away
  • Ovalis - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    . The Wireless switch and the device are toofar away from each other. Place the Wireless switch in a position closer tothe device. The Wireless switch lost pairing. Pair the device again. Refer to• Socket outlet, page 9 < 0,5 s 10 DUG_Ovalis SSO_WH-06 Ovalis - Connected single socket outlet 16A https
  • Insights+

    Wiser Home – System User Guide (UK, Ireland)

    over past months. You can view savings in £ or kWh. It also displays savings from Away Mode and Eco Mode, with an option to enable Eco Mode for additional savings. How the weather affects your heating (F) This section shows how weather impacts your heating system's performance. We consider the
  • EVlink Home Smart Device user guide

    automatically or at scheduled times. By using the Wiser Homeapp, you can create automations based on your needs. Creating an automationThe following is an example of creating an automation to start the EV Chargerwhen you are away. NOTE: EV Charger can only act as an action. 1. On the Home page, tap . 2. Go
  • Wiser Motion Sensor Wiser Home Device user guide

    condition is met. 4. Tap Add conditions and select any of the following (C):– Device status change: Select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For
  • Configuración avanzada del dispositivo

    Termostato Conectado Wiser 2 A – Wiser Home Guía del usuario del dispositivo

    sobre la duración de la ocupación. Cuando se ha activado la detección de presencia o el retroceso, la pantalla de matriz de puntos del termostato muestra el modo "away" como a continuación indica la detección de entrada. Ejemplo de modo de calefacción: Si el usuario establece el punto de ajuste del
Page 24 of 33