Showing 231 - 240 of 1,457 results

Page 24 of 146
  • Væk-tilstand

    LK FUGA® Wiser trådløs PIR-lysdæmper med nul – Brugervejledning til Wiser Home-enheden

  • Wiser Home AI

    Wiser Home – System User Guide (Spain and Portugal)

    Override Function (Away Mode): Overrides the Wiser Home AI function to adapt your home settings when you are away, ensuring energy efficiency even when you're not home. Notifications for Feature Malfunction: Notifies you in case of a feature malfunctions. Supported devices: Power Micromodule (Water
  • Modo ausente

    Unica - Detetor de movimento com interruptor 10A conectável – Guia do utilizador do dispositivo Wiser Home

  • Borta-läge

    Exxact - Ansluten rörelsesensor med tryckknappsdimmer med lysdioder – Bruksanvisning för Wiser Home-enhet

  • Væk-tilstand

    LK FUGA® Wiser trådløst dobbeltrelæ – Brugervejledning til Wiser Home-enheden

  • Advanced device settings

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    , thermostat dot matrix display shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° C Celsius and the inputs detect room occupancy, the thermostat will adhere to the 23° C setpoint. However, if the room becomes unoccupied
  • Advanced device settings

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    , thermostat dot matrix display shows away mode as below indicating input detection. Example for heating mode: If the user sets the thermostat's setpoint to 23° C Celsius and the inputs detect room occupancy, the thermostat will adhere to the 23° C setpoint. However, if the room becomes unoccupied
  • Afwezigheidsmodus

    Wiser Home – Systeem gebruikshandleiding (België)

  • Modo ausente

    Unica - Detetor de movimento variador LED conectável – Guia do utilizador do dispositivo Wiser Home

  • Modo Ausente

    Unica - Detector de movimiento con regulador LED conectado – Guía del usuario del dispositivo Wiser Home

Page 24 of 146