Showing 3,231 - 3,240 of 9,859 results

Page 324 of 986
  • Reading the System User Guide Online

    Wiser Home – System User Guide (UK, Ireland)

    . A Table of Contents Tap/Click to navigate through the topics. Tap/Click the + and - icons to expand/collapse a chapter. B Document name Tap/Click to navigate to the first page of the document. C PDF Icon Tap/Click to open the document as a PDF file. D Search field Enter a search term and tap/click
  • Aikataulun määrittäminen

    Exxact – Liiketunnistin Multiwire LED-säätimellä Zigbee – Wiser Home -laitteen käyttöopas

    luodaksesi aikataulun. Anna aikataulun nimi (A). Valitse TYYPPI-valikosta Valot (B). Valitse KOSKEE-valikossa Liiketunnistin himmentimellä (C) laiteluettelosta. Napauta Luo määrittääksesi tapahtumia. Valitse TAPAHTUMAT (D) -valikossa päivä, ja napauta sitten lisätäksesi tapahtuman, kuten TILA
  • Sensor de inundación Wiser Guía del usuario del dispositivo Wiser Home

    en este documento contiene descripciones generales,características técnicas o recomendaciones relacionadas con productos osoluciones. Este documento no pretende sustituir a un estudio detallado o un plan de desarrollo oesquemático específico de operaciones o sitios. No debe usarse para determinar
  • Safety Information

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure. The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are
  • Safety Information

    Ovalis - Connected Relay Switch 10 A – Wiser Home Device user guide

    or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure. The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are
  • Colocar o modo de conforto sazonal em pausa

    Unica - Comando de estores conectável – Guia do utilizador do dispositivo Wiser Home

    Colocar o modo de conforto sazonal em pausa Colocar o modo de conforto sazonal em pausa Colocar o modo de conforto sazonal em pausa Através da aplicação Wiser Home, pode definir a posição do estore e colocar o modo de conforto sazonal em pausa durante algum tempo. Para colocar o modo de conforto
  • Managing shutter operation without temperature sensor

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed. To define the
  • Datos técnicos

    Control PowerTag – Guía del usuario del dispositivo

    Datos técnicos Datos técnicos Datos técnicos Principales características Fuente de alimentación 230 V CA ± 20 % Frecuencia 50/60 Hz Consumo máximo IO ≤ 2 VA 2DI ≤ 3 VA Temperatura de funcionamiento de -25 °C a +60 °C Temperatura de almacenamiento de -40 °C a +85 °C Humedad relativa (60068-2-78) 93
  • Definir as definições lux

    Unica - Detetor de movimento com interruptor 10A conectável – Guia do utilizador do dispositivo Wiser Home

    Definir as definições lux Definir as definições lux Definir as definições lux Pode definir o valor limite para intervalos de lux (como muito escuro, escuro, claro e muito claro) do ambiente. Isto evitará a deteção falsa causada por alterações na intensidade da luz. No ecrã Inicial, toque em . Toque
  • Managing shutter operation without temperature sensor

    Ovalis - Connected Blind Control Switch – Wiser Home Device user guide

    Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Managing shutter operation without temperature sensor Using the Wiser Home app, you can manage the shutter operation of a room where no temperature sensor is installed. To define the
Page 324 of 986