Showing 341 - 350 of 1,457 results

Page 35 of 146
  • Criar uma automatização

    Plenum Airzone e Aidoo Pro - Ar condicionado – Guia do utilizador do dispositivo Wiser Home

    ) para definir a condição. Se tiver selecionado a condição como Modo ausente e a ação como Controlar um dispositivo, esta automatização irá sobrepor-se às definições do Away Mode. Selecione as opções que pretende configurar: Toque em (F) e arraste a barra deslizante para cima/baixo (G) para ajustar a
  • Schneider Charge Wiser Home Device user guide

    of the following (D): – Device status change (Select the device)– Away Mode (Enable or Disable)– Energy Price changes (To define the energy price limit.) NOTE: This condition is available only if your tariff is set to Peak/Off-Peak or Dynamic. Refer to Setting Tariff. NOTE: Maximum 10 conditions can
  • Wiser Water Leakage Sensor Wiser Home Device user guide

    : Select a device to enable automation.– Away Mode: Enable / Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the shutter etc. For more information about AwayMode, refer to the system user guide. e.g. Good Morning If When
  • About the device

    Wiser Plug – Wiser Home Device User Guide

    devices further away from the Wiser Hub. Advantage of using the Plug: Configure several time schedules to switch on/off the Plug. Set notification to alarm when power consumption (high or low). Features of the Plug: Mobile or manual control anytime, anywhere with the Wiser app Works with Amazon Alexa, the Google Assistant and Siri Diagram of operating elements A. On/Off button
  • Exxact - Connected Double Socket Outlet 16A Wiser Home Device user guide

    - Connected Double Socket Outlet 16A 4. Tap Add conditions (B) and select any of the following (C). – Device status change (Select the device): An automation will be triggeredbased on a device status, such as the opening of a shutter or the detectionof movement by a motion sensor. – Away Mode (Enable
  • Exxact - Connected Single Socket Outlet 16 A Wiser Home Device user guide

    movement by a motion sensor. – Away Mode (Enable or Disable): Away mode can also trigger anautomation to turn on the lights, close the shutter etc. For more informationabout Away Mode, refer to the system user guide. NOTE: Maximum 10 conditions can be added. New automation If When Conditions are met All
  • Micro Module Shades Control (Puck)

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    /Reset button 5 times in quick succession on the Puck. Short press the mechanical double push button 1 for 5 times in quick succession. The status LED blinks green on the Puck. If the Puck is located away from the mechanical push button, the status LED might not be visible. The shutter will move up and down a few times. The status LED stops blinking green on the Wireless switch and the Puck. The Puck can now be controlled by the Wireless switch.
  • Insights+

    Wiser Home – System User Guide (UK, Ireland)

    over past months. You can view savings in £ or kWh. It also displays savings from Away Mode and Eco Mode, with an option to enable Eco Mode for additional savings. How the weather affects your heating (F) This section shows how weather impacts your heating system's performance. We consider the
  • Exxact - Connected Motion Sensor with Push-button Dimmer LED

    Away Mode Away Mode Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Voice control Voice control Using Amazon Alexa™ or Google Home, you can control the device with your voice. Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France
  • Wiser Underfloor Heating Controller / Connection Strip Wiser Home Device user guide

    Controller / Connection Strip 4. Tap Add conditions and select any of the following (C): – Device status change: Select a device to enable automation.– Away Mode: Enable/Disable away mode to trigger an action. TIP: Away mode can also be used as a trigger to turn off the lights,dimmer or closing the
Page 35 of 146