DUG_LK FUGA Wiser Wireless Switch_WH-00

Micro Module Shades Control (Puck)

  1. If you do not need the lower rocker of the Wireless switch, you can replace it with a blind plate.
  2. Remove the top rocker and short press the left push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  3. WARNING
    HAZARD OF ELECTRIC SHOCK
    • Observe the regulations for working on live parts.
    • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    Follow either of the options to pair the Puck:
    • Short press the Setup/Reset button 5 times in quick succession on the Puck.
    • Short press the mechanical double push button 1 for 5 times in quick succession.
    The status LED blinks green on the Puck.
    NOTE: If the Puck is located away from the mechanical push button, the status LED might not be visible.

    The shutter will move up and down a few times. The status LED stops blinking green on the Wireless switch and the Puck. The Puck can now be controlled by the Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?