Showing 491 - 500 of 1,457 results

Page 50 of 146
  • Silencing the device

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    Silencing the device Silencing the device Silencing the device Hush the smoke alarms During an alarm event, first identify the smoke alarm/s that detected smoke, these will have Red LEDs blinking. Then short press the Test/Hush button on the smoke alarm to stop the alarm. In hush mode, the smoke
  • Operating modes

    Wiser Micromodule for Fil Pilote radiators – Wiser Home Device User Guide

    Operating modes Operating modes Operating modes Using the Wiser Home app, you can control the Heating devices. On the Control tab, tap All devices or a room tab where the Plug is located > Heating device. On the Device Control screen, the current temperature is shown. The current operating mode
  • Eco-läge

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    Eco-läge Eco-läge Eco-läge Eco Mode är en smart funktion utformad för att maximera effektiviteten i ditt värmesystem. Det optimerar automatiskt stopptiden för uppvärmningsfasen varje gång den inställda temperaturen ändras från ett högre till ett lägre värde. Eco Mode är en systemfunktion som
  • Silencing the device

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    Silencing the device Silencing the device Silencing the device Hush the smoke alarms During an alarm event, first identify the smoke alarm/s that detected smoke, these will have Red LEDs blinking. Then short press the Test/Hush button on the smoke alarm to stop the alarm. In hush mode, the smoke
  • Ovalis - Interrupteur de commande de volet connecté Guide de l'utilisateur de l’appareil Wiser Home

    %3Atrue&term=Away+Mode 5. Pour lancer l’automatisme à un moment donné, appuyez sur Quand >Ajouter un horaire et sélectionnez l’une des options suivantes (D) : NOTE: Vous pouvez ajouter jusqu’à 10 entrées de temps. – Heure précise de la journée - L’automatisme se déclenche à une heureprécise de la journée
  • Tehostustila

    Wiser Home – Järjestelmän käyttöopas (Ruotsi, Suomi)

  • Changing the device from 1-gang to 2-gang

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Changing the device from 1-gang to 2-gang Changing the device from 1-gang to 2-gang Changing the device from 1-gang to 2-gang You can change the Wireless switch mode from 1-gang to 2-gang before you pair your device to the Hub/Gateway. The Wireless switch is in 1-gang mode by default. Follow the
  • LED Indication

    LK One Wiser Multiwire LED Rotary Dimmer – Wiser Home Device user guide

    LED Indication LED Indication LED Indication Pairing User Action LED Indication Status Press the push button 3 times. LED blinks amber per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning off. Resetting User Action LED Indication
  • Boost-läge

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

  • Troubleshooting

    Wiser Micro Module Dimmer – Wiser Home Device user guide

    . Reduce load. Change load. Check wiring between the push button and the Puck. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set RL LED mode (it is advised
Page 50 of 146