Showing 5,091 - 5,100 of 9,846 results

Page 510 of 985
  • Identifying the device

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Identifying the device Identifying the device Identifying the device Using the Wiser Home app, you can identify the thermostat from the other available devices in the room. On the Home screen, tap . Tap Devices Flush Mount Thermostat Room settings Identify (A). The thermostat LEDs on the dot-matrix display flash white while the wireless connectivity LED flashes green at the same until you tap Ok.
  • Tietoja laitteesta

    Exxact - Huone/lattiatermostaatti 16 A ZB – Wiser verhokytkin -laitteen käyttöopas

    Tietoja laitteesta Tietoja laitteesta Tietoja laitteesta Huone/lattiatermostaattia 16 A ZB (jäljempänä cFMT/termostaatti) käytetään pääasiassa lattiasähkölämmitykseen tai sähköpattereihin, mutta sitä voidaan käyttää myös sähköverkkokäyttöisten moottorisoitujen venttiilien tai vesipohjaisen
  • Tietoja laitteesta

    Renova - Huone/lattiatermostaatti 16 A ZB – Wiser verhokytkin -laitteen käyttöopas

    Tietoja laitteesta Tietoja laitteesta Tietoja laitteesta Huone/lattiatermostaattia 16 A ZB (jäljempänä cFMT/termostaatti) käytetään pääasiassa lattiasähkölämmitykseen tai sähköpattereihin, mutta sitä voidaan käyttää myös sähköverkkokäyttöisten moottorisoitujen venttiilien tai vesipohjaisen
  • Removing the Aidoo Pro Heat Pump

    Airzone - Aidoo Pro Heat Pump – Wiser Home Device user guide

    Removing the Aidoo Pro Heat Pump Removing the Aidoo Pro Heat Pump Removing the Aidoo Pro Heat Pump To remove the Aidoo Pro Heat Pump from the Wiser Home app: On the Control tab, tap All devices or a room tab where the Aidoo Pro Heat Pump is located and select the Aidoo Pro Heat Pump under the name you assigned (A). Tap > Device settings > Delete. Tap OK after reading the confirmation message.
  • Felsökning

    Exxact – Rörelsedetektor med tryckknapp 10 A uppkopplad – Bruksanvisning för Wiser Home-enhet

  • Amazon Alexa™

    Exxact – Rörelsedetektor med tryckknapp 10 A uppkopplad – Bruksanvisning för Wiser Home-enhet

  • Insights

    Wiser Home – System User Guide (France)

    Insights Insights Insights The Insights feature gives you multiple features in a single place. This includes energy saving, system activity, heating time and access to your heat report. To navigate to Insights from the Home screen: Tap Insights (A) If you have an energy device or energy monitoring device installed at your home, Energy Centre will be displayed.
  • Automation

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Automation Automation Automation An automation allows you to trigger an action automatically or at scheduled times when certain conditions are met. By using the Wiser Home app, you can create automations based on your needs. This example demonstrates how a device works when the condition is met.
  • Automatização

    Unica - Interruptor conectável – Guia do utilizador do dispositivo Wiser Home

    Automatização Automatização Automatização Uma automatização permite-lhe acionar uma ação automaticamente ou às horas agendadas quando determinadas condições estão preenchidas. Ao utilizar a aplicação Wiser Home, pode criar automatizações com base nas suas necessidades. Este exemplo mostra como funciona um dispositivo quando a condição está preenchida.
  • Deleting an automation

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    Deleting an automation Deleting an automation Deleting an automation On the Home screen, tap Automations . Go to Automation, tap the automation you want to delete. On the Edit automation screen, tap Delete automation (A) and read the confirmation message and then tap OK (B).
Page 510 of 985