DUG_Exxact - ZB Thermostat 16 A_WH-01

Identifying the device

Using the Wiser Home app, you can identify the thermostat from the other available devices in the room.
  1. On the Home screen, tap .
  2. Tap Devices > Flush Mount Thermostat > Room settings > Identify (A).
    NOTE: The thermostat LEDs on the dot-matrix display flash white while the wireless connectivity LED flashes green at the same until you tap Ok.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?