Showing 5,331 - 5,340 of 9,846 results

Page 534 of 985
  • Lisäasetukset

    PowerTag Energy – Wiser Home Laitteen käyttöopas

    olet poistanut aurinkoenergiajärjestelmän, napauta (A) ja valitse Ei. Jos olet määrittänyt PowerTagin aurinkoenergiaksi tai aurinkoenergiaksi/akuksi (yhdistelmä), (A) kenttä Onko sinulla aurinkopaneelit? poistetaan käytöstä. Katso lisätietoja laitteen pariliittämisestä
  • Installieren des Geräts

    System M und System D - Connected Raumtemperaturregler 2 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    Installieren des Geräts Installieren des Geräts Installieren des Geräts Weitere Informationen finden Sie in der Installationsanleitung für den Connected Raumtemperaturregler-Einsatz, 2 A, die mit diesem Produkt geliefert wird. Siehe die Installationsanleitung für den Connected Raumtemperaturregler
  • Troubleshooting in Quick Home Connect

    LK FUGA Wiser Push-button Switch – Wiser Home Device user guide

    -button switch The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button switch The
  • Troubleshooting in Quick Home Connect

    LK One Wiser Push-button Switch – Wiser Home Device user guide

    -button switch The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button switch The
  • Troubleshooting in Quick Home Connect

    LK FUGA Wiser Multiwire LED Push-button Dimmer – Wiser Home Device user guide

    -button dimmer The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button dimmer The
  • Troubleshooting in Quick Home Connect

    LK One Wiser Multiwire LED Rotary Dimmer – Wiser Home Device user guide

    dimmer The Wireless switch is not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Rotary dimmer The Wireless switch
  • Using the device

    Exxact - Connected Motion Sensor with Push-button Dimmer LED – Wiser Home Device user guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off , adjust the brightness level and control various settings. On the Control tab, select Motion Sensor Dimmer. The Device Control Screen displays the following options: A Tap to turn the device on
  • Using the device

    LK FUGA® Wiser wireless PIR with relay – Wiser Home Device user guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off of the Motion Sensor Switch and control various settings. On the Control tab, select Motion Sensor Switch. The Device Control Screen displays the following options: A Tap to turn the device on
  • Configuración avanzada

    Control PowerTag – Guía del usuario del dispositivo

    establece inicialmente durante el emparejamiento. Si le parece que la configuración no es correcta, recomendamos quitar el Control PowerTag del sistema Wiser y volver a ponerlo en marcha con la opción/configuración correcta.Consulte: Emparejamiento del dispositivo Eliminación del dispositivo En la
  • Remover o dispositivo

    Controlador temperatura 16A Wiser – Guia do utilizador do dispositivo

    Remover o dispositivo Remover o dispositivo Remover o dispositivo Com a aplicação Wiser Home, pode remover o relé do sistema Wiser. Para remover o relé: No ecrã Inicial, toque em . Toque em Dispositivos Relé 16A Excluir (A).
Page 534 of 985