DUG_Micro Module Shades Control_WH-08

Identifying the device

Using the Wiser Home app, identify the Puck among the devices available in a home.
  1. On the Home screen, tap .
  2. Tap Devices > Shutters > Micromodule Shutter or Shutter slat > Identify (A).
    The status LED blinks red and the shutter opens/closes gradually, upon successful identification of the Puck or shutter slat.
  3. Tap OK to finish identifying the device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.