Showing 5,401 - 5,410 of 9,846 results

Page 541 of 985
  • Resetting the device

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    successful reset, the LED stops blinking. Then, the device restarts and blinks green for a few seconds. All configuration data, user data and network data are deleted. After reset, the LED turns amber, indicating that the socket is ready for pairing.
  • Caractéristiques techniques

    Actionneur de Chaudière Wiser – Guide de l'utilisateur de l’appareil Wiser Home

    Caractéristiques techniques Caractéristiques techniques Caractéristiques techniques Tension du principale : 220-240 V CA, 50 Hz Capacité nominale du commutateur : 2 (1) A, 230 V CA charge totale max. 2,5 A Câblage : Câblage fixe uniquement Interface utilisateur : 2x boutons-poussoirs / LED
  • Editing an automation

    Wiser Boiler Relay – Wiser Home Device user guide

    the settings. To remove a condition, slide the condition towards left and then tap (A) to delete it. Tap ⊕ Add conditions (B) to add new condition. To change the order of actions, tap the Then option, and hold an action, then drag and drop to the desired position. Tap Save to save the changes.
  • Fjernelse af enheden

    Wiser bevægelsessensor – Brugervejledning til Wiser Home-enheden

    Fjernelse af enheden Fjernelse af enheden Fjernelse af enheden Med Wiser Home-appen kan du fjerne sensoren fra Wiser-systemet. Tryk på på Hjem skærmen. Tryk på Enheder Bevægelsessensor Slet (A). Derudover kan du fjerne sensoren fra Wiser-systemet ved at trykke på fanen Styring Bevægelsessensor
  • Ta bort enheten

    Wiser magnetkontakt för fönster och dörr – Bruksanvisning för Wiser Home-enhet

    Ta bort enheten Ta bort enheten Ta bort enheten Med Wiser Home-appen kan du ta bort sensorn från Wiser-systemet. Tryck ikonen på startskärmen. Tryck på Enheter Fönster-/dörrsensor Radera (A). Du kan dessutom ta bort sensorn från Wiser-systemet genom att trycka på fliken Kontroll Fönster-/dörrsensor
  • Editing an automation

    Wiser Window/Door Sensor – Wiser Home Device user guide

    the settings. To remove a condition, slide the condition towards left and then tap (A) to delete it. Tap ⊕ Add conditions (B) to add new condition. To change the order of actions, tap the Then option, and hold an action, then drag and drop to the desired position. Tap Save to save the changes.
  • Editing an automation

    Ovalis - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    the settings. To remove a condition, slide the condition towards left and then tap (A) to delete it. Tap ⊕ Add conditions (B) to add new condition. To change the order of actions, tap the Then option, and hold an action, then drag and drop to the desired position. Tap Save to save the changes.
  • Setting the device location

    Ovalis - Connected Relay Switch 10 A – Wiser Home Device user guide

    open setup screen. On the Device Setup screen, you can enter New room name (A) or select an existing room from the list (B). If the device is already assigned, you can remove it from the existing room. Tap Remove from Room (C). Once changes are done, tap Submit (D).
  • Handling QR code Issues

    Wiser Home – System User Guide (Germany, Austria)

    Handling QR code Issues Handling QR code Issues Handling QR code Issues Condition Action If you are unable to find the QR code. Tap I can't find the correct QR code and proceed to Adding a Device. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR
  • Getting to Know the Wiser System

    Wiser Home – System User Guide (Germany, Austria)

    reports for connected Wiser devices. With a personal account and the Wiser Home App on a smartphone you can control and monitor connected Wiser devices from anywhere where the internet is available for both mobile phone and the Hub.
Page 541 of 985