Showing 5,461 - 5,470 of 9,846 results

Page 547 of 985
  • Identifiering av enheten

    Wiser temperatur och luftfuktighetssensor – Bruksanvisning för Wiser Home-enhet

    -/luftfuktighetsgivare Identifiera (A). Dessutom kan du identifiera sensorn genom att trycka på fliken Kontroll Temperatur-/luftfuktighetsgivare Enhetsinställningar Identifiera (A). Sensorlampan blinkar för att identifiera sensorn och fortsätter att blinka grönt tills du trycker på OK.
  • Using the device

    Wiser Water Leakage Sensor – Wiser Home Device user guide

    Using the device Using the device Using the device The Control Panel of the Sensor allows you to monitor the current status of water leakage detection. On the Control tab, tap All devices or a room tab where the sensor is located On the Sensor control panel page, you can see the following: Water leakage status (A) History (B) Device settings (C) Add to favourites (D)
  • Troubleshooting

    Wiser Water Leakage Sensor – Wiser Home Device user guide

    sensor is reporting status. The firmware update runs in the background. LED blinks amber with a beep sound. The sensor battery is low or drained. Replace the battery in the device A notification pop–up will appear on the app.
  • Technical Data

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    External fuse protection 10 A circuit breaker Nominal current 4 A, cosφ = 0.6 Operating frequency 2405 - 2480 MHz Max. radio-frequency power transmitted < 10 mW Communication protocol Zigbee 3.0 certified
  • Eliminación del dispositivo del sistema

    System M y Sistema D - Toma de corriente inteligente, 1 elemento, 16 A – Guía del usuario del dispositivo Wiser Home

    Eliminación del dispositivo del sistema Eliminación del dispositivo del sistema Eliminación del dispositivo del sistema En la aplicación Wiser Home, puede eliminar una toma de corriente del sistema Wiser. Eliminación de la toma de corriente: En la página principal, toque . Toque Dispositivos Enchufe conectado Eliminar (A).
  • Removing the device from Wiser system

    PowerTag Energy – Wiser Home Device user guide

    Removing the device from Wiser system Removing the device from Wiser system Removing the device from Wiser system Using the Wiser app, you can remove the PowerTag from the system. On the Home screen, tap . Tap Devices > Energy and select a PowerTag from the list. Tap Delete (A). Tap Remove from System. All the historical data will be deleted from the app.
  • Historial

    Wiser Home – Guía del usuario del sistema (España y Portugal)

    y años) pulsando (A). La importación de la red se muestra en azul y el exceso de energía solar y de batería se muestra en verde. Puede tocar y seleccionar Consumo de carga para ver la energía consumida por las diferentes cargas. Toque (A) y seleccione el período de tiempo deseado.
  • Editing Schedule/Event

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    Editing Schedule/Event Editing Schedule/Event Editing Schedule/Event To edit the schedule: On the Home screen, tap . Tap Schedules tab and select the Schedule that you want to modify. Tap SCHEDULE DETAILS to do any of the following: To rename the device To change the device location To delete Schedule To edit the EVENTS, select a day, and tap to change the time and temperature.
  • Eliminación del dispositivo

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    Eliminación del dispositivo Eliminación del dispositivo Eliminación del dispositivo Con la app Wiser Home, puede eliminar el termostato del sistema Wiser. Para eliminar el termostato del sistema Wiser: En la página Inicio, toque . Toque Dispositivos Eliminar (A). Lea el mensaje de confirmación y
  • Funcionamiento manual

    Micromódulo regulador Wiser LED – Manual del usuario del dispositivo Wiser Home

    Funcionamiento manual Funcionamiento manual Funcionamiento manual Cuando el módulo está conectado a un botón pulsador mecánico, los dispositivos de iluminación conectados se pueden controlar manualmente. Pulsación corta del pulsador mecánico -1 para encender/apagar la luz. Pulse y mantenga pulsado
Page 547 of 985