Showing 5,581 - 5,590 of 9,846 results

Page 559 of 985
  • Resetting the device

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    reset, the LED stops blinking. Then, the device restarts and blinks green for a few seconds. After reset, the LED turns amber indicating that it is ready for pairing.
  • Ligar/desligar o dispositivo através da aplicação

    Unica - Botão variador de luz LED conectável – Wiser Home Dispositivo Guia do utilizador

    Ligar/desligar o dispositivo através da aplicação Ligar/desligar o dispositivo através da aplicação Ligar/desligar o dispositivo através da aplicação No separador Controlo, toque em Todos os dispositivos ou no separador Divisão, onde se encontra o variador. Toque em (A) para ligar/desligar o regulador de intensidade. Também pode ligar/desligar o dispositivo e ajustar o brilho a partir do ecrã Casa quando o adicionar aos seus Favoritos.
  • Caractéristiques techniques

    Unica - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    d’extension Boutons-poussoirs mécaniques doubles, nombre illimité, max. 50 m Protection externe par fusible disjoncteur 10 A Courant nominal 4 A, cosφ = 0,6 Fréquence de fonctionnement 2405 - 2480 MHz Puissance de radiofréquence max. transmise < 10 mW Protocole de communication certifié Zigbee 3.0
  • Shutter with tilting slats

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    Shutter with tilting slats Shutter with tilting slats Shutter with tilting slats On the Home screen, tap . Tap Devices Shutters Shutter with tilting slats. Tap Open duration/ Close duration (A) and enter the recorded shutter opening/closing time. Tap (B) and enter the slat tilt duration according
  • Supervisión del consumo de energía

    System M y Sistema D - Toma de corriente inteligente, 1 elemento, 16 A – Guía del usuario del dispositivo Wiser Home

    corriente está encendida, el consumo de energía se muestra en vatios (W). El consumo de potencia varía en función de la carga conectada a la toma de corriente.
  • Zeitplan/Ereignis bearbeiten

    System M und System D - Connected Raumtemperaturregler 2 A, ZB – Wiser Home Geräte-Benutzerhandbuch

  • Testing the individual device

    Wiser Smoke Alarm - Battery – Wiser Home Device user guide

    Testing the individual device Testing the individual device Testing the individual device Test the smoke alarm once a month to ensure proper operation. If the smoke alarm is installed in a mobile home, test weekly and before every journey.Press the Test/Hush button on each smoke alarm for more than
  • Shutter with tilting slats

    Odace - Connected Blind Control Switch – Wiser Home Device user guide

    Shutter with tilting slats Shutter with tilting slats Shutter with tilting slats On the Home screen, tap . Tap Devices Shutters Shutter with tilting slats. Tap Open duration/ Close duration (A) and enter the recorded shutter opening/closing time. Tap (B) and enter the slat tilt duration according
  • Identification de l’appareil

    Odace - Thermostat connecté filaire 2 A – Guide de l'utilisateur de l’appareil Wiser Home

    Identification de l’appareil Identification de l’appareil Identification de l’appareil À l’aide de l’application Wiser Home, vous pouvez identifier le thermostat à partir des autres appareils disponibles dans la pièce. Sur l’écran d’ accueil, appuyez sur . Appuyez sur Appareils Identification (A
  • Configuración del hub

    Wiser Home – Guía del usuario del sistema (España y Portugal)

    Configuración del hub Configuración del hub Configuración del hub Para poder controlar el sistema a través de su smartphone, el hub debe estar conectado a Internet. Puede configurar el hub utilizando la aplicación como Propietario de la casa e Instalador profesional. La aplicación ofrece el menú
Page 559 of 985