Showing 561 - 570 of 1,100 results

Page 57 of 110
  • About the device

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    features: Measure & control the room temperature Dot-matrix displays (current room and set temperature) Device lock Valve Protection Heat/cool changeover Universal input setback/presence (external) Volt-free or live control, normally open or normally closed. Smart schedule through a Wiser app
  • Mode de charge

    EVlink Home Smart – Guide d'utilisation de l'appareil Wiser Home

    Mode de charge Mode de charge Mode de charge À l’aide de l’application Wiser Home, vous pouvez gérer le mode de charge. Dans l'onglet Control, appuyez sur Tous les appareils > EVlink Home Smart. Sur la page du panneau de commande de l’appareil, appuyez sur Mode de charge. Dans le menu EV
  • Modo de carregamento

    EVlink Home Smart – Manual do utilizador do dispositivo doméstico Wiser

    Modo de carregamento Modo de carregamento Modo de carregamento Através da aplicação Wiser Home, pode gerir o modo de carregamento. No separador Controlo, toque em Todos os dispositivos > EVlink Home Smart. Na página do painel de controlo do dispositivo, toque em Modo de carregamento. No menu EV
  • Insights

    Wiser Home – System User Guide (Spain and Portugal)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Insights

    Wiser Home – System User Guide (Sweden, Finland)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Google Home™

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Google Home™ Google Home™ Google Home™ Google Home™ is a brand of smart speakers that work similarly to Amazon’s Alexa. The user can speak a profusion of commands to request information, or ask Google Assistant to perform action.” Common Wiser commands for Google Home™: Inquiry: “OK, Google, is the
  • About the device

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
  • Modo de carga

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    Modo de carga Modo de carga Modo de carga Con la aplicación Wiser Home, puede administrar el modo de carga. En la pestaña Control, pulse Todos los dispositivos > EVlink Home Smart. En la página del panel de control del dispositivo, toque Modo de carga. En el menú EV Charging Mode, seleccione una
  • Insights

    Wiser Home – System User Guide (Denmark)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Seasonal Comfort-tila asettaminen

    Wiser verhomoduuli ZB – Wiser Home -laitteen käyttöopas

    kalibrointiin suljintyypin mukaan Napauta Home -näytössä Smart Modes Seasonal Comfort Mode. Seasonal Comfort-tila -asetussivu avautuu, jossa voit päivittää seuraavat asetukset: Voit muuttaa Seasonal Comfort-tila asetuksia seuraavasti: A Seasonal Comfort-tila: Napauta kytkintä kytkeäksesi Seasonal
Page 57 of 110