DUG_Radiator Thermostat_WH-07

Google Home™

Google Home™ is a brand of smart speakers that work similarly to Amazon’s Alexa. The user can speak a profusion of commands to request information, or ask Google Assistant to perform action.”

Common Wiser commands for Google Home™:

  • Inquiry: “OK, Google, is the hot water on?”

  • Hot Water Command: “OK, Google, turn on/off the hot water”

  • Room Temperature: “OK, Google, how warm is (room name)?”

  • Set Temperature: “OK, Google, set (room name) to XX degrees”

  • Increase Temperature: “OK, Google, increase the setpoint by XX degrees”

  • Set Temperature: “OK, Google, set (room name) to XX degree”

Changes made with Google Home™

All changes made through a voice command related to radiator thermostat that is valid for one hour, or until the next scheduled event. The user cannot change this action. This also applies for boosts initiated from the radiator thermostat.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?