SUG_DA_WH-04

Insights

The Insights provides information on the annual bill for the tariff set. It helps to keep track of your energy.

NOTE: The option to set a tariff is only available if you have an Energy device installed in your home. For more information, please refer to the Device User Guide of the respective device.

  1. For a more detailed overview, tap Energy costs (A).

    Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or resistive Water boilers (controlled with a Wiser Power Micromodule). It relies on users to answer routine questions. Refer to Wiser Home AI for detailed information.

  2. You can change the displayed timeframe (days, months and years).

    IMPORTANT: If you have installed PowerTag on solar or solar with battery My savings is available to view savings and earning history.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.