Showing 61 - 70 of 1,473 results

Page 7 of 148
  • Mode Absence

    Wiser Tête de Vanne Thermostatique – Guide de l'utilisateur de l’appareil Wiser Home

    Mode Absence Mode Absence Mode Absence Lorsque le mode Absence (A) est activé, toutes les pièces sont réglées sur la température d’absence (par défaut 16 °C). Une coche s’affiche dans la page « Automatismes » en cas d’activation. Vous trouverez cette page dans le menu « Automatismes », en appuyant
  • Example of an automation

    Wiser Smart Plug 16A – Wiser Home Device User Guide

    Example of an automation Example of an automation Example of an automation In the example below, if away mode is enabled during Daytime, then Plug will turn off. Go to Automation > to create an automation. To add a condition, tap Add Condition > Away Mode > Enabled away mode (A). Read the
  • Indbygget automatisering

    Wiser radiator termostat – Brugervejledning til Wiser Home-enheden

  • Mode Absence

    Wiser Home – Guide de l’utilisateur du système (France)

    Mode Absence Mode Absence Mode Absence Le mode Absence est conçu pour placer votre domicile dans un état sensible lorsque vous partez pour des périodes prolongées (p. ex. lorsque vous êtes absent pour le week-end). Il remplace temporairement la commande normale (p. ex. moments, automatismes) mise
  • POISSA KOTOA -tila

    Exxact - Huone/lattiatermostaatti 16 A ZB – Wiser verhokytkin -laitteen käyttöopas

  • Creating an Automation

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    : Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode , refer to the System User Guide. Tap Device status change > . Set
  • Creating an Automation

    Wiser Radiator Thermostat 2nd Generation – Wiser Home Device user guide

    : Select a device to enable automation. Away Mode: Enable/Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode , refer to the System User Guide. Tap Device status change > . Set
  • App Settings

    Wiser Home – System User Guide (UK, Ireland)

    List of all Devices of your Home. Access to Device options. Away Mode Specify what happens when you activate the Away Mode, like temperature setting and which devices should be switched off. Refer to Away Mode for detailed information. Smart Modes Activate or deactivate the Smart Modes, like ECO
  • Creating an automation

    Wiser Micro Module Shades Control – Wiser Home Device user guide

    triggers an action when at least one condition is met. Tap Add conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable / Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or
  • Creating an automation

    Wiser Water Leakage Sensor – Wiser Home Device user guide

    conditions and select any of the following (C): Device status change: Select a device to enable automation. Away Mode: Enable / Disable away mode to trigger an action. Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode
Page 7 of 148