Showing 721 - 730 of 1,241 results

Page 73 of 125
  • Creating an automation

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    actions within an automation. In this example, we will initially select Control a device and select Smart Socket (F) as the device to trigger an action, later, we will select for the Wait option to add a delay in the automation. You cannot select the same device that you selected for Add conditions in
  • Anti-Tripping-Management

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    wird, werden die Zeitpläne, Momente und Automatisierung für dieses Gerät nicht ausgeführt. Es können maximal 8 Geräte hinzugefügt werden. Unterstützte Geräte: Lastaktor (Warmwasserbereiter) Smart Plug Smarte Steckdosen Schneider Charge Voraussetzung: Konfigurieren Sie eines Ihrer Geräte PowerTag als
  • Informações técnicas

    EVlink Home Smart – Manual do utilizador do dispositivo doméstico Wiser

    Informações técnicas Informações técnicas Informações técnicas EVlink Home Smart Gama EVlink Home Nome do produto EVlink Home Smart Tipo de produto Estação de carregamento CA Descrição do polo 3P + N para o circuito de potência 1P + N para o circuito de potência Modo de montagem Montado na parede
  • Creating an automation

    LK FUGA® - Wiser wireless socket outlet 1½ M – Wiser Home Device user guide

    within an automation. In this example, we will initially select Control a device and select Smart Socket (F) as the device to trigger an action, later, we will select for the Wait option to add a delay in the automation. You cannot select the same device that you selected for Add conditions in Step 4
  • Installation af enheden

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

  • About the device

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    Universal input setback/presence (external) Volt-free or live control, normally open or normally closed. Smart schedule through a Wiser app Operating elements Dot-matrix display Wireless connectivity LED ( ) Heating demand LED ( ) All LED indications are explained in the LED Indications. Rotary push-button
  • Apparater

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    enheter, t.ex. golvlampor, radioapparater, ventilatorer eller kaffemaskiner, med appen. Övervaka energiförbrukningen för anslutna enheter. Bruksanvisning (PDF) Användarhandbok 2-vägsuttag 16A WDE002182 WDE003382 WDE004384 Består av ett smart- och ett standarduttag. Det övre smarta uttaget styr och övervakar den inkopplade strömmen. Det nedre standarduttaget tillhandahåller effekt som inte är styrd eller övervakad. Bruksanvisning (PDF) Användarhandbok
  • Creating an automation

    Wiser Smart Plug 16A – Wiser Home Device User Guide

    wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation. Tap Control a device > Smart Plug, tap (F) to turn on/off, then tap Set. Maximum 10 actions can be added. To remove an action, swipe left on the action
  • Wiser Home System User Guide (Sweden, Finland)

    you areaway for added security Show me Not for me ShutterLiving room Openuntil 16:00 Automations SUG_SV_FI_WH-04 63 Configuring the Wiser System 3. Tap Devices. List of Devices: Back Settings Account Rooms Devices Away Mode Smart Modes System settings Support Home Screen App VersionX.Y.Z (Build XX
Page 73 of 125