Showing 741 - 750 of 1,241 results

Page 75 of 125
  • Troubleshooting

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    , to prevent airflow from affecting sensor performance. The thermostat has gone offline. The thermostat is not On. The thermostat is no longer in signal range of the Hub. Turn the thermostat On and Off. Move the Wiser Hub closer to the thermostat. Use Wiser Smart plug to increase the range. Unable to
  • Troubleshooting

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    , to prevent airflow from affecting sensor performance. The thermostat has gone offline. The thermostat is not On. The thermostat is no longer in signal range of the Hub. Turn the thermostat On and Off. Move the Wiser Hub closer to the thermostat. Use Wiser Smart plug to increase the range. Unable to
  • Troubleshooting

    Schneider Charge – Wiser Home Device user guide

    following the procedure described in section "Operation". Connector plugged into electric vehicle but not charging, LED is blinking blue. Verify that you do not have a schedule in progress through the smart charging application that prevents charging the car. If you have installed the anti-tripping
  • Energy

    Wiser Home – System User Guide (Germany, Austria)

    PowerTag C A9XMC1D3 Control and monitoring wireless communication module Instruction Sheet Device User Guide EVlink Home Smart EVH4xxxN EVH4xxxNC Supplies electric energy to charge plug-in electric vehicles Instruction Sheet Device User Guide Schneider Charge EVH5A22N2S EVH5A11N2CX EVH5A07N2CX
  • Setting up a schedule

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Setting up a schedule

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Configuring UFH actuator

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    temperature.The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or ELKO - Smart Radiator Thermostat. Refer, pairing the device. Refer, . Assign a room to the thermostat once it has been paired and then tap Next to configure
  • Setting up a schedule

    Exxact - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Instalación del dispositivo

    Enchufe inalámbrico Wiser 16A – Guía del usuario del dispositivo Wiser Home

  • Skapa en automation

    Wiser Smart kontakt 16 A – Användarhandbok för Wiser Home-enhet

    automation. Tryck på Styra en enhet > Smart kontakt, tryck på (F) för att slå på/stänga av, tryck sedan på Ställ in. Högst 10 åtgärder kan läggas till. Om du vill ta bort en åtgärd sveper du åt vänster på åtgärden och trycker på . Ange namnet på automationen (G). Du kan välja den höljesbild som motsvarar
Page 75 of 125