Showing 8,091 - 8,100 of 9,967 results

Page 810 of 997
  • Modification d’un automatisme

    PowerTag Control – Guide de l’utilisateur de l’appareil

    suivantes : Changer l’icône . Renommer l’automatisme. Appuyer sur chaque condition pour modifier les paramètres. Pour supprimer une condition, faites-la glisser vers la gauche, puis appuyez sur (A) pour la supprimer. Appuyez sur ⊕ Ajouter une condition (B) pour ajouter une nouvelle condition. Pour
  • Connecting Devices to the Hub

    Wiser Home – System User Guide (Sweden, Finland)

    Connecting Devices to the Hub Connecting Devices to the Hub Connecting Devices to the Hub For the Wiser devices to be controlled by the hub, they must be connected to the hub. Connecting devices to the hub is part of the set up process. You can add devices to the hub at any time. The app guides you through the process of adding devices. You can find detailed information about the necessary steps for adding the device in the chapter Adding a Device.
  • Insights

    Wiser Home – Järjestelmän käyttöopas (Ruotsi, Suomi)

    yksityiskohtaisemman yleiskatsauksen, napauta Energiakustannukset (A). Ota Wiser Home AI ­‑ominaisuus käyttöön napauttamalla palkkia (B). Wiser Home AI on ominaisuus, jonka avulla käyttäjät voivat pienentää sähkökustannuksia rekisteröimällä korkean energian laitteet, kuten sähköauton laturi (EVlink Home Smart
  • Använda enheten

    Wiser Brandvarnare 230V – Bruksanvisning för Wiser Home-enhet

    brandvarnarens kontrollpanel: Brandvarnarens aktuella tillstånd (A) Historik (B) Historiksidan innehåller information brandvarnaren enheten (datum, tid och typ av larm som identifierats. Mer information finns i Kontrollera enhetshistoriken). Enhetsinställningar (C) På sidan med brandvarnarinställningar finns information om hur du ställer in brandvarnarens ljusstyrka. Mer information finns i Inställningar för LED-ljusstyrka. Lägg till i favoriter (D)
  • Connecting Devices to the Hub

    Wiser Home – System User Guide (UK, Ireland)

    Connecting Devices to the Hub Connecting Devices to the Hub Connecting Devices to the Hub For the Wiser devices to be controlled by the hub, they must be connected to the hub. Connecting devices to the hub is part of the set up process. You can add devices to the hub at any time. The app guides you through the process of adding devices. You can find detailed information about the necessary steps for adding the device in the chapter Adding a Device.
  • Away Mode

    Wiser Home – System User Guide (UK, Ireland)

    Away Mode Away Mode Away Mode The Away Mode is designed to set your home in a state that is sensible when you are away for longer periods of time (e.g. being away for the weekend). It temporarily overrides the normal control (e.g. moments, automation) implemented in the hub. When you disable the
  • Troubleshooting

    Schneider Inverter and Boost – Wiser Home Device user guide

    Troubleshooting Troubleshooting Troubleshooting A. If the connection cannot be established, check the following points: The device is powered. The serial number is correct. You are located in the vicinity of the inverter. B. If you are still having trouble reconnecting the device, follow the steps
  • Cambio de localización

    Sensor de movimiento de exterior ARGUS 360 – Guía del usuario del dispositivo Wiser Home

    Cambio de localización Cambio de localización Cambio de localización Con la aplicación Wiser Home puede cambiar la localización del sensor de movimiento. En la página Detalles del dispositivo, toque en Localización. En la página de ajustes, puede introducir Nuevo nombre de la habitación (A) o
  • Modification de l'emplacement

    Capteur de mouvement extérieur ARGUS 360 – Guide de l'utilisateur de l’appareil Wiser Home

    Nouveau nom de pièce (A) ou sélectionnez une pièce existante dans la liste (B). Si l’appareil est déjà affecté, vous pouvez appuyer sur Supprimer de la pièce (C) pour le supprimer de la pièce existante. Une fois les modifications effectuées, appuyez sur Envoyer (D) pour confirmer l'emplacement du capteur de mouvement.
  • Modification d’un automatisme

    Capteur de mouvement extérieur ARGUS 360 – Guide de l'utilisateur de l’appareil Wiser Home

    l’automatisme que vous souhaitez modifier. Vous pouvez désormais effectuer les modifications suivantes: Changer l’icône. Renommer l’automatisme. Appuyer sur chaque condition pour modifier les paramètres. Pour supprimer une condition, faites-la glisser vers la gauche, puis appuyez sur (A) pour la supprimer. Appuyez sur Ajouter des conditions (B) pour ajouter une nouvelle condition. Appuyez sur Sauvegarder pour sauvegarder les modifications.
Page 810 of 997