DUG_Inverter and Storage_WH-03

Troubleshooting

A. If the connection cannot be established, check the following points:

  • The device is powered.

  • The serial number is correct.

  • You are located in the vicinity of the inverter.

B. If you are still having trouble reconnecting the device, follow the steps below to re-establish an expired Bluetooth connection and repeat the process:

  • Unscrew the collar on top of the dongle.

  • Unplug the dongle from the inverter.

  • Plug the dongle back into the inverter.

  • Tighten the screw back into place.
    Once re-attached, the “PWR” and “COM” lights on the dongle will be solid green.

If you are still having trouble reconnecting the device, please visit our Support Pages.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?